Custom STM32WB55 Project workflow
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-13 2:46 AM
Hello everyone,
ive bought a Nucleo STM32WB55 evaluation board (MB1355C) + Dongle (MB1293C), which ive played around a bit for a while now with trying out different examples from the STM32Cube_FW_WB_V1.5.0 Firmware package.
My goal is to use the STM32WB55 on a custom board (which ive already layouted) in a battery powered application to transfer a constant stream of data (ADC values) to the Nucleo Board (MB1355C) , which should act as a GATT Server, and the custom board should be the GATT Client.
Would it be feasible to use the examples from the firmware package (i.e. "BLE_DataThroughput") and to modify them for my application, or would it be better to start from scratch using CubeMX for my custom board? Or is there any other, better way?
- Labels:
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-14 2:27 AM
If your custom board is sending data to the Nucleo board, then your board is a GATT server and the Nucleo board is a GATT Client.
BLE_DataThroughput project is the project using the bigger size of data exchanged in between a server and client.
You can start from it and add the data capture inside a custom task.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-14 2:45 AM
Ill try that. Thank you very much.
Also, is there a way to get rid of the "button push" for the pairing process or is this mandatory due to the bluetooth protocol implementation? It would be nice if both the custom board and the nucleo board would pair automatically once both are powered up.