cancel
Showing results for 
Search instead for 
Did you mean: 

I'm going to run a ping-pong example with two p-nucleo-lrwan1.

yjae
Associate II

I'm going to run a ping-pong example with two p-nucleo-lrwan1. How do I separate the master from the slave? Terminal uses 'tera Term'.

2 REPLIES 2

The first unit running becomes the master, and a secondary unit receiving the message switches to slave mode. There can be some meta-stability and you can likely alter the state by resetting.

The basic test here is that they transmit back and forth and see each other.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
yjae
Associate II

Thank you. I want to check if it works like ping-pong exemple in the p-nucleo-lrwan1 manual. However, the terminal does not show the 'it's 0:0:3:930 WU@ 0:0:4:930'.Is this right?