cancel
Showing results for 
Search instead for 
Did you mean: 

I cannot completely turn off STM32Le55 (RAK3172)

lino
Associate
 

I'm using a micro stm32wl55 (RAK3172). I try to shut it down using shutdown mode. By turning it off without ever using the PWR_SUBGHZSPICR command, the micro turns on and off regularly with the expected consumption. However, if I activate the PWR_SUBGHZSPICR command even just once, after the shutdown the consumption remains high and I can no longer turn it off completely. Could you give me a solution? Thank you 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @lino 

The command PWR_SUBGHZSPICR doesn't exist. But we have the PWR_SUBGHZSPICR_NSS which I used to perform testes on Low_Power_Modes using an STM32WL55JC1 Nucleo Board. Everything works Fine. Can You give more details.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.