Skip to main content
Kampi
Associate III
November 23, 2023
Question

Porting ZigBee TempMeas_Client_Router to custom board with ZigBee2MQTT support

  • November 23, 2023
  • 1 reply
  • 1325 views

Hi,

I´m trying to port the example from above to my custom sensor board and use ZigBee2MQTT together with this board. You can find the code in the attachments.

The board connects via ZigBee, but can not report the config

[M4 APPLICATION] ZbStartup Callback (status = 0x00)
[M4 APPLICATION] [TEMP MEAS] Report Config Failed error:148
[M4 APPLICATION] APP_ZIGBEE_Init
[M4 APPLICATION] **********************************************************
[M4 APPLICATION] WIRELESS COPROCESSOR FW:
[M4 APPLICATION] VERSION ID = 1.17.0
[M4 APPLICATION] FW Type : FFD Zigbee stack
[M4 APPLICATION] Application flashed: ..
[M4 APPLICATION] Channel used: 11
[M4 APPLICATION] Link Key: ZigBeeAlliance09
[M4 APPLICATION] Link Key value: 5a 69 67 42 65 65 41 6c 6c 69 61 6e 63 65 30 39
[M4 APPLICATION] Clusters allocated are:
[M4 APPLICATION] Temperature measurement Client on Endpoint 17
[M4 APPLICATION] **********************************************************
[M0] [00000000.000][API] Init_ZigbeeStack_Infrastructure
[M4 APPLICATION] APP_ZIGBEE_StackLayersInit
[M4 APPLICATION] Network config : APP_STARTUP_CENTRALIZED_ROUTER
[M0] [00000000.022][PLATFORM] ZbNlmeResetReq : NLME-RESET.request (warmStart = 0)
[M0] [00000000.018][PLATFORM] zb_startup_join_nwk_disc : Attempting network discovery. Scans = 3, Duration = 4
[M0] [00000000.019][PLATFORM] nwk_scan_req : MLME-SCAN.request (wpan0): type=1, page=0, mask=0x00000800, dur=4
[M0] [00000000.030][PLATFORM] nwk_handle_beacon_ind : BEACON addr16=0x0000, epid=0x00124b001cdfee60, ch=11, pan=0x1a62, depth= 0, lqi=206, cost=1, pjoin=1
[M0] [00000000.287][PLATFORM] nwk_scan_req : MLME-SCAN.request (wpan0): type=1, page=0, mask=0x00000800, dur=4
[M0] [00000000.299][PLATFORM] nwk_handle_beacon_ind : BEACON addr16=0x0000, epid=0x00124b001cdfee60, ch=11, pan=0x1a62, depth= 0, lqi=206, cost=1, pjoin=1
[M0] [00000000.557][PLATFORM] nwk_scan_req : MLME-SCAN.request (wpan0): type=1, page=0, mask=0x00000800, dur=4
[M0] [00000000.569][PLATFORM] nwk_handle_beacon_ind : BEACON addr16=0x0000, epid=0x00124b001cdfee60, ch=11, pan=0x1a62, depth= 0, lqi=206, cost=1, pjoin=1
[M0] [00000000.018][PLATFORM] nwk_join_try_next : Associating (src=0x0080e12500e0a24b) to 0x0000 (epid = 0x00124b001cdfee60, lqi = 206, ch = 11)
[M0] [00000000.619][PLATFORM] ZbMonitorHandleTransKeyInd : Adding network key, sequence number = 0
[M0] [00000000.621][PLATFORM] ZbZdoDeviceAnnce : Sending Device_Annce for 0xa758
[M4 APPLICATION] ZbStartup Callback (status = 0x00)
[M4 APPLICATION] Stop
[M4 APPLICATION] [TEMP MEAS] Report Config Failed error: 0x94
[M4 APPLICATION] Start

What is the reason for this?

Also the timer from the Time Server isn´t started, because the timer callback isn´t called when I press the start button. What is the reason for this error?

This topic has been closed for replies.

1 reply

ST Technical Moderator
January 5, 2024

Hello @Kampi ,

From the source code the reporting is configured correctly on the router side, the application is working properly with a WB coordinator using the app TempMeas_Server_Coord.

For me, the issue may be located on the coord side.

When using the reporting from the client side with the API function ZbZclAttrReportConfigReq, Binding entry will be added on server side automatically. Looking at your logs, the error code returned corresponds to ZCL_STATUS_TIMEOUT = 0x94 meaning that no binding entry is added by the server.

What is the configuration on the server side ? ( the cluster used should be configured as a server )

Did you try the same test with a WB nucelo board as a coordinator ?

BR,
Ouadi