2021-03-22 01:00 AM
I tried to debug the code by changing the "CFG_DEBUGGER_SUPPORTED" to 1 , but still we are facing the issues, RTOS tasks are not executing as expected. We found some task in ble_app.c with priority of "osPriorityNone" which is 0. Does this example code has any issue?
2021-03-25 05:45 AM
hi, @SMane.2 (Community Member)
In BLE_HeartRateFreeRTOS example code GPIO Pins( PB5 for LED1, PB0 for LED2 and PB1 for LED3) are not initialized as GPIO output mode.
GPIO_InitTypeDef GPIO_InitStruct = {0};
/*Configure GPIO pins : LD2_Pin LD3_Pin LD1_Pin */
GPIO_InitStruct.Pin = LED1_PIN|LED2_PIN|LED3_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
HAL_GPIO_WritePin(GPIOB, LED1_PIN|LED2_PIN|LED3_PIN, GPIO_PIN_RESET);
2021-03-26 12:46 AM
Thanks,@Aishwarya
I already added this things in the MX_GPIO_Init() function, but still it was not working. It was going in task only single time. Now I changed "CFG_LPM_SUPPORTED" to 0. So after disabling the LOW Power Mode, now its executing all task properly. Is low power mode making any problem to RTOS task? How can I optimize power? and implement sleep modes with BLE & RTOS both?
2021-04-05 07:13 AM
1
2021-10-06 09:15 AM
I am finding the same issue, did anyone find a solution to this problem?
2021-10-07 03:41 AM
hi @Community member After disabling the LOW Power Mode, the problem resolved(CFG_LPM_SUPPORTED = 0). If you want low power mode enabled(CFG_LPM_SUPPORTED = 1) you can change this "configEXPECTED_IDLE_TIME_BEFORE_SLEEP" parameter, On code regeneration it will be 2. You can increase to 10 to 30 Ticks as per your requirement. In FreeRTOS.h file you will find this parameter