cancel
Showing results for 
Search instead for 
Did you mean: 

How to use USB/UART/BLE stack with sequencer?

dnj
Associate III

I have problem with USB stack as Virtual Port COM to use it with sequencer prepared to BLE stack. I mean I don't know how to execute needed CDC... functions inside usbd_cdc_if.c. Did anybod do that?

I want to send via UART and via BLE received through USB VCP.

Any Application Notes to do that?


_legacyfs_online_stmicro_images_0693W00000dJpIoQAK.png

1 REPLY 1
FBL
ST Employee

Hi @dnj 

USBD_CDC_ItfTypeDef defines the interface for CDC class on firmware. Each of the functions corresponds to a callback that should be called during operation. As far as I know, to implement a CDC VCP with sequencer, is like implementing it in as task in an OS. The following example does not use an OS:

STM32CubeWB/Projects/P-NUCLEO-WB55.Nucleo/Applications/USB_Device/CDC_Standalone at master · STMicroelectronics/STM32CubeWB (github.com)

 

I hope this would be helpful

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


I'm out of offce with limited access to my emails.
Happy New Year!