Skip to main content
GBehe
Associate III
August 19, 2020
Question

How to use the EEPROM emulation example code "EEPROM_Emul" from"X-CUBE-EEPROM_V2.0.0" package on a custom STM32WB55CE board.

  • August 19, 2020
  • 30 replies
  • 14286 views

I have my custom STM32WB55CE board. I had programmed the example code "EEPROM_Emul" from"X-CUBE-EEPROM_V2.0.0" package on it. It was working fine. Then I did FUS upgrade with BLE full stack binary programming on it. After that, the same EEPROM emulation example code gets stuck at EE_Init() function. It goes into Hardfault handler. I did a FLASH erase and reprogrammed the example code. On my STM32WB55 Neucleo board, it works fine. Please guide on this.

Thank you.

This topic has been closed for replies.

30 replies

Remi QUINTIN
ST Technical Moderator
August 19, 2020

​>I did a FLASH erase and reprogrammed the example code

Did rework?

EE_Init()  => may be blocked when trying to perform the first flash accesses.

Which WB FW package version are you using?

You upgrade the RF stack, not the FUS.. correct?

GBehe
GBeheAuthor
Associate III
August 19, 2020

Hi Remi.

Thanks for such a quick response.

Sorry, I did not get "Did rework?" - I just did Flash erase operation - all sectors (in STLink Utility) and again programmed the EEPROM emulation example code.

I am not aware about blocking during first flash accesses .

Regarding FUS, first time I did upgrade with FUS fs 1.0.2 after performing a Firmware Delete operation(In STM32Cube Programmer(GUI)). And programmed BLE_Stack_full_fw.bin and it was successful. When I did these same procedures again, it failed. I also tried with STM32Cube Programmer(CLI). It still failed. Even BLE stack programming failed. Apart from these two binaries upgrade, I did not do anything else.

I always tried to program BLE full fw stack.

Next , I tried EEPROM emulation example code again.

Thanks.

Remi QUINTIN
ST Technical Moderator
August 19, 2020

Sorry => Did it rework? I was asking whether the example code was running OK again.

>When I did these same procedures again, it failed => This is expected. The FUS never accepts the reprograming of the same version as the one already installed. Only new upgraded version can be programed. There is an anti-rollback mechanism that prevents any old (or same) FUS version to be reinstalled.

When I got issues like yours, I always perform a mass erase of the flash memory in order to start from a clean state.

This can be done via the 2 lines in a batch file in CLI mode

CLI.exe -c port=swd -ob RDP=0xBB

CLI.exe -c port=swd -rdu

Or using the mass erase feature available in the CubeProgrammer tool in GUI mode.

Then the upload of the RF stack should be OK.

GBehe
GBeheAuthor
Associate III
August 19, 2020

Got it. But is't it strange that the BLE stack also is not getting programmed?

And, is there anything from FUS upgrade side effecting EEPROM Emulation not working as I am facing now?

I am asking it, because on my board. the example was working, I did debug it two times. After the FUS and BLE binary upgrades I found my issue.

Thank you.

GBehe
GBeheAuthor
Associate III
August 20, 2020

To do a mass erase, I tried first using CUBE programmer GUI. It doesn't provide the option when my device is connected. You an see the screenshot.

GBehe
GBeheAuthor
Associate III
August 20, 2020

Then I tried doing it in STlink utility. It also ailed. Screenshot attached.

Log:

10:57:45 : ST-LINK SN : 066EFF545150656767240731

10:57:45 : ST-LINK Firmware version : V2J36M26

10:57:45 : Connected via SWD.

10:57:45 : SWD Frequency = 4,0 MHz.

10:57:45 : Connection mode : Connect Under Reset.

10:57:45 : Debug in Low Power mode enabled.

10:57:45 : Device ID:0x495 

10:57:45 : Device flash Size : 1MBytes

10:57:45 : Device family :STM32WBxx

10:59:28 : [SAFIN_peripherals_test_latest.bin] opened successfully.

10:59:28 : [SAFIN_peripherals_test_latest.bin] checksum : 0x00605EF4 

11:05:19 : Error occured during flash mass erase!

11:19:39 : Disconnected from device.

GBehe
GBeheAuthor
Associate III
August 20, 2020

If I do sector erase, It works but does not show any success message. The log is below.

11:29:25 : ST-LINK SN : 066EFF545150656767240731

11:29:25 : ST-LINK Firmware version : V2J36M26

11:29:25 : Connected via SWD.

11:29:25 : SWD Frequency = 4,0 MHz.

11:29:25 : Connection mode : Connect Under Reset.

11:29:25 : Debug in Low Power mode enabled.

11:29:25 : Device ID:0x495 

11:29:25 : Device flash Size : 1MBytes

11:29:25 : Device family :STM32WBxx

11:31:40 : ST-LINK SN : 066EFF545150656767240731

11:31:40 : ST-LINK Firmware version : V2J36M26

11:31:40 : Connected via SWD.

11:31:40 : SWD Frequency = 4,0 MHz.

11:31:40 : Connection mode : Connect Under Reset.

11:31:40 : Debug in Low Power mode enabled.

11:31:40 : Device ID:0x495 

11:31:40 : Device flash Size : 1MBytes

11:31:40 : Device family :STM32WBxx

Does it mean Flash erase was successful?

Again, I performed those commands you had mentioned, in Cube programmer CLI. They worked fine. You can see in the screenshot.

GBehe
GBeheAuthor
Associate III
August 20, 2020

The command for memory read protection disabling also worked.

But after this, I did not perform the FUS upgrade and Radio stack binaries programming. And I did EEPROM emulation example programming, thinking that lets do it freshly. It's still going to Hard Fault handler in the EE_Init() function.

Thanks.

GBehe
GBeheAuthor
Associate III
August 20, 2020

After this, I did not do any FUS and Radio stack updates. And BLE Heart rate example project is working. I am able to connect from my Mobile and access data.

Strange.

Remi QUINTIN
ST Technical Moderator
August 20, 2020

​Using CubeProgrammer, the mass erase is achieved checking the "Select" option to select all sectors.

Then click on "Erase selected sectors". It must work!