2021-09-28 3:31 AM
/*SPI Initialization*/
static void MX_SPI1_Init(void)
{
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;//SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;//SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;//SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
/*RGB LED CONTROL*/
HAL_GPIO_WritePin(GPIOH, GPIO_PIN_1, GPIO_PIN_SET);
HAL_Delay(100);
HAL_SPI_Transmit(&hspi1, "0x3A", 1, 100);
HAL_SPI_Transmit(&hspi1, "0x7F", 1, 100);
HAL_SPI_Transmit(&hspi1, "0x00", 1, 100);
HAL_SPI_Transmit(&hspi1, "0x00", 1, 100);
Hi I am using STM32WB5MMG-DK for my project development activities. I wanted to control RGB LED(LD4). Is there any code example which to perform the required operation?
2021-09-28 6:00 AM
> HAL_SPI_Transmit(&hspi1, "0x3A", 1, 100);
This is a string value with 4 characters in it (plus a null terminator). Your code actually sends the ASCII character "0" here.
If you want to send the value 58 (0x3A), don't use the quotes. You also need to pass a pointer to the value rather than raw data.
uint8_t data = 0x3A;
HAL_SPI_Transmit(&hspi1, &data, 1, 100);
Also, if PH1 is a CS line, it should be high (set) before the transaction and low (reset) just prior to sending data. Not sure of it's function here.