2020-10-08 01:36 AM
Hello there !
When I use Monitor RF to upgrade firmware(0x7000 offset on CPU1) and wireless stack (0xF000 offset on CPU2) trough OTA : It works.
But when I want to upgrade (or just rewrite the same version of FUS) trough OTA at 0xF000 on CPU2 : it doesn't works... After upgrading, it seems the board is blocked, and it's impossible to discover it...
Why ?
Thanks in advance,
Matt
2020-10-13 01:52 AM
No one ?
2020-10-22 06:56 AM
Updating the same FUS version always generates an error. this error message results from the anti-rollback system that prevents reverting to the same or older version of the FUS.
2020-10-22 09:11 AM
Could you download the option bytes, expecially SFSA and SBRV?
What is the FUS version you wanted to upgrade? V1.1.0 on a V1.0.2?