2021-05-21 10:44 AM
Hello everyone,
I'm new here, but already made a few developpment on a ST32F7 chip, but now have a question about USB and virtual COM.
Is it possible to use the second USB port of the NUCLEO board to make a virtual COM and manage communication with a PC ? I mean, without using STLINK USB port.
If so, could you please explain how to do that, and if there are some example and application notes I can find ?
Hoping someone may help me and give some recommendations.
Have a nice day,
Kindly
Patrick
Solved! Go to Solution.
2021-05-25 1:29 PM
Hello Patrick,
I would like to welcome you to the ST community. Yeah it is not a problem to connect other USB connector on STM32WB55 nucleo and communicate with computer. You are looking for example called CDC_Standalone which can be found in the STM32CubeWB FW package. Further information how to set it up could be found in our video tutorial on this topic MOOC - STM32 USB training . Please click on Select as Best next to my answer if you will find this materials helpful.
2021-05-25 1:29 PM
Hello Patrick,
I would like to welcome you to the ST community. Yeah it is not a problem to connect other USB connector on STM32WB55 nucleo and communicate with computer. You are looking for example called CDC_Standalone which can be found in the STM32CubeWB FW package. Further information how to set it up could be found in our video tutorial on this topic MOOC - STM32 USB training . Please click on Select as Best next to my answer if you will find this materials helpful.
2021-05-27 11:09 PM
Hello Petr,
THank's a lot for your answer, this is exactly what I was looking for !
In fact, I couldn't find such an example because I was looking only in the Examples folders, not in the Applications one...
I tested it and also followed the MOOC you suggested.
All is right for me now on this topic.
Have a nice day, and than's again !
Patrick