How to run examples provided by MCU software packages
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-27 8:51 AM
Hello,
I'm a beginner with STM32CubeIDE environment and I'm having a lot of troubles trying to run Application examples download from the STM32Cube MCU Packages.
What is the right way to import projects. As an example I'm trying to import the BLE_p2pServer_ota from the STM32Cube_FW_WB_V1.2.0 software package using "import" from CubeIDE. However after the project is imported I cannot build it.
The target is not set automatically as should be. I suppose that examples are pre-configured for the target board, but it isn't.
I have tried on Windows and Mac but I get the same issues. The process is not straightforward.
Do you have any suggestions?
Thanks
Labels:
- Labels:
-
STM32CubeIDE
-
STM32WB series
0 REPLIES 0