How to receive SPI data from MAX31855 with Nucleo WB55 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-05 1:48 AM
Hello,
I use a Nucleo WB55 and I would like to receive temperature data from MAX31855.
The protocol used is SPI.
1) Connections
Firstly I tested the MAX31855 with an Arduino and I managed to get data. I used the same MAX31855 and double-checked the wires between the Nucleo and the MAX and this seems good. I chose SPI1 (NSS = PA4 / SCK = PA5 / MISO = PA6).
I think that these connections are right.
2) SPI mode
Regarding the MAX chronogram, I think that the right mode is 0.
3) Configuration file IOC
Data Size is limited to 16 bits but the MAX sends 32bits. Is it ok if I use twice HAL_SPI_Receive_DMA() ?
(Full code is available at point 4)
uint8_t pData1[2] = {0};
uint8_t pData2[2] = {0};
...
HAL_SPI_Receive_DMA(hspi, pData1, 2);
HAL_SPI_Receive_DMA(hspi, pData2, 2);
SCK Rise and Fall time is 200ns. so I made this operation to find the baud rate :
Baud Rate = 1 bit / SCK Rise and Fall time = 1/(200 x 10^-9) = 5 x 10^-6 = 5Mbits/s
In IOC file, the maximum baud rate (Prescaler = 2) is 2Mbits/s which is not enough.
How can I set a good baud rate?
DMA configuration :
4) Code
main.c :
int main(void)
{
HAL_Init();
SystemClock_Config();
PeriphCommonClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_SPI1_Init();
/* USER CODE BEGIN WHILE */
//LED2 OFF
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET);
HAL_StatusTypeDef status;
while (1)
{
/* USER CODE BEGIN 3 */
status = HAL_SPI_Init(&hspi1);
blinkLed2();
Get_SPI1_DMA_Data(&hspi1);
blinkLed2();
}
/* USER CODE END 3 */
}
spi.h :
#ifndef INC_SPI_H_
#define INC_SPI_H_
#include "stm32wbxx_hal.h"
#define SPI_SCK_PIN GPIO_PIN_5
#define SPI_MISO_PIN GPIO_PIN_6
#define SPI_CS_PIN GPIO_PIN_4
#define SPI_GPIO_PORT GPIOA
void blinkLed2(void);
void Get_SPI1_DMA_Data(SPI_HandleTypeDef *hspi);
void Get_SPI1_Polling_Data(SPI_HandleTypeDef *hspi);
#endif /* INC_SPI_H_ */
spi.c :
#include "spi.h"
#include "main.h"
uint8_t overflow = 0;
uint8_t pData1[2] = {0};
uint8_t pData2[2] = {0};
void blinkLed2(void)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET);
HAL_Delay(500);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET);
HAL_Delay(500);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET);
HAL_Delay(500);
}
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
overflow = 1;
}
void Get_SPI1_DMA_Data(SPI_HandleTypeDef *hspi)
{
HAL_GPIO_WritePin(SPI_GPIO_PORT, SPI_CS_PIN, GPIO_PIN_RESET);
//HAL_Delay(500);
HAL_SPI_Receive_DMA(hspi, pData1, 2);
HAL_SPI_Receive_DMA(hspi, pData2, 2);
HAL_Delay(500);
HAL_GPIO_WritePin(SPI_GPIO_PORT, SPI_CS_PIN, GPIO_PIN_SET);
HAL_Delay(500);
if (overflow == 1)
{
//[32:18] = Temp
//[17] = Reserved, always 0
//[16] = 0(OK)/1(Fault)
//[15:4] = Cold junction temp
//[3] = Reserved, always 0
//[2] = 0(OK)/1(SCV Fault = Short-circuited to VCC)
//[1] = 0(OK)/1(SCG Fault = Short-circuited to GND)
//[0] = 0(OK)/1(OC Fault = Open thermocouple)
}
overflow = 0;
}
Have a nice day
Laora
- Labels:
-
SPI
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-05 2:13 AM
I forgot to show the data output :
Here is the data mapping :