2021-07-13 12:19 AM
I am trying to power B-L072Z-LRWAN1 board using CN11 USB connector but not able to power it. Though I am able to see Red Led (LD7) glowing, Lorawan stack is not getting executed. I think MCU is not powered. Does anyone know how to power with CN11 connector?
2021-09-22 12:35 AM
Hi all,
Can anyone explain the way to power the board with batteries?
I am trying with a small LED blink application. The board is working fine with the St-link power but not working with the batteries.
The above image is taken from the user manual of the same board. Where I am doing wrong?
2021-09-22 3:08 PM
Not seeing any images
"If the board is supplied by CN13, by battery or by CN11, SB37 must be removed to release the RESET pin managed by ST-LINK. In that case the ST-LINK is no more powered."
2021-09-22 9:13 PM
Thank you for the reply...
But I don't want to ST-Link to be removed so I thought it is fine if I don't remove SB37.
The missing image is there below. this statement is right above the statement you shared.
I have gone through the schematic and I tried Closing (Fitting) the SB5 and it worked. Is it a bad approach?
2021-09-22 9:40 PM
Its less about powering, and more about not letting the ST-LINK clamp the device in reset.
The ST-LINK SWDIO/SWCLK pins are still connected.
2021-09-22 10:02 PM
Can you please elaborate it?