cancel
Showing results for 
Search instead for 
Did you mean: 

How to get the firmware&code for Lora GW inside of P-NUCLEO-LRWAN3?

hzhao.11
Associate

I have a P-NUCLEO-LRWAN3 toolkit and I would like to know how I can get the firmware&code for Lora GW which is runing on NUCLEO-F746ZG. The I-CUBE-LRWAN only contain that for Lora End Node which is running on NUCLEO-L073RZ.

In the document DM00620948 I see the follow words "The gateway firmware binary is available upon request directly from STMicroelectronics.". So I would like to know if I can get the newest firmware(current I'm using "2.1.7, Nov 6 2018").

What's more, is the source code of gateway firmware available to me? I want to add some extra logic on gateway. I'll be highly appreciate if you could provide the source(source with libraries is also accessable).

Thank you!

1 REPLY 1

Probably has NDA and/or SLA associated with it, contact your local sales office for details.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..