2022-02-23 12:21 AM
In STOP2 mode, the current of STM32WB5MMG is around 170uA at 3V.
Using the same FW (based on the HeartRate example), the P-NUCLEO-WB55 can achieve a low current (approximately 3 uA).
Is there any additional settings for STM32WB5MMG?
Solved! Go to Solution.
2022-03-17 09:30 AM
Hello,
If you measure the current on the STM32WB5MMG Discovery Kit, it is a known problem. Indeed, the ST-Link supply is connected on STM32WB5MMG supply, so there is an overconsumption. This issue will be corrected on the next version of this board.
Best Regards
2022-02-28 09:03 PM
The pull-up register of PH3-BOOT0 pin affects the current.
On our board, PH3-BOOT0 is connected to VDD with pull-up register according to datasheet of STM32WB5MMG.
If we remove the pull-up register, the current goes down.
Is there any pull-down register in the STM32WB5MMG at PH3-BOOT0 pin?
On P-NUCLEO-WB55 and STM32WB5MM-DK, PH3-BOOT0 is connected to GND with pull-down register.
PH3-BOOT0 should be connected to GND with pull-down register?
2022-03-17 09:30 AM
Hello,
If you measure the current on the STM32WB5MMG Discovery Kit, it is a known problem. Indeed, the ST-Link supply is connected on STM32WB5MMG supply, so there is an overconsumption. This issue will be corrected on the next version of this board.
Best Regards