2023-01-14 5:30 AM
We made custome PCB board using STM32WB5MMG. We tried (489) BLE Security with STM32WB - 04 Simple BLE application generated from CubeMX - YouTube, and also we followed repository example too. We enabled the necessary settings which is mentioned above video but weI didn't get BLE name.
2023-01-18 1:41 AM
Hello,
If you try to flash the BLE_HeartRate example available in STM32CubeWB package with the stm32wb5x_BLE_Stack_full_fw.bin binary on the Wireless Coprocessor, is it working or not?
Best Regards
2023-01-18 5:05 AM
Hello,
Yes, now it's working. Thank you for being so supportive.
2023-01-28 3:08 AM
I am facing the same issue the program is flashed but not able to find the ble i just followed
2023-01-28 10:54 PM
i am also facing the same issue please help us
2023-01-28 11:07 PM
stm32wb5x_BLE_Stack_full_fw.bin binary on the Wireless Coprocessor what does this line means
2023-01-28 11:12 PM
make: *** No rule to make target 'C:/Users/ashut/Desktop/heart_rate/BLE_HeartRate/Drivers/STM32WBxx_HAL_Driver/Src/stm32wbxx_hal_qspi.c', needed by 'Drivers/STM32WBxx_HAL_Driver/stm32wbxx_hal_qspi.o'. Stop. getting this error
2023-01-30 1:17 AM
Hello,
You can look the following wiki page which describes how to setup your board to use BLE examples. The BLE_HeartRate example requires having the stm32wb5x_BLE_Stack_full_fw.bin binary flashed on the CPU2.
Best Regards
2023-01-30 1:20 AM
Hello,
To enable the QSPI module, you should uncomment the following define in stm32wbxx_hal_conf.h file:
/*#define HAL_QSPI_MODULE_ENABLED */
Best Regards