High frequency uplink with STM32WLE5JC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 5:11 AM
Hello,
I am working on a project using the STM32WLE5JC module and STM32CubeIDE for development, with firmware packge v.1.3.0.
We are currently running EMC tests at a test facility, and they have requested for the ability for the device to send data every 500ms (to The Things Network, TTN). Is this doable? What configuration will be needed to accomplish such a fast transmission rate?
Thanks
Solved! Go to Solution.
- Labels:
-
STM32WL series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 6:17 AM
@helixembedded wrote:to The Things Network, TTN
As @Uwe Bonnes said, pretty sure this would break TTN's terms of use?
But, surely, what network you use is of no concern to the test house?
Surely, you just need to transmit - can't you adjust the Ping-Pong example for that?
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 5:55 AM
Last time i looked, TTN has a limit of 1000 message/day or 30 seconds of airtime/day. whatever is less. Your requirment for sure breaks this limit.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 6:17 AM
@helixembedded wrote:to The Things Network, TTN
As @Uwe Bonnes said, pretty sure this would break TTN's terms of use?
But, surely, what network you use is of no concern to the test house?
Surely, you just need to transmit - can't you adjust the Ping-Pong example for that?
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 6:25 AM
The network is definitely not an issue here - we just need to transmit.
I was not aware of the Ping Pong example code. Will it be able to send data that quickly?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 6:52 AM
@helixembedded wrote:Will it be able to send data that quickly?
I don't see why not - it's just a very simple demo ...
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 8:15 AM
Hello @helixembedded
First the Ping Pong example is a point-to-point application and not a transmission from an End node to network (such as TTN). So, you can't use it for a transmission to a Gateway.
For your case, on the End Node example, set the #define APP_TX_DUTYCYCLE to 500. If you will have an issue, it should be an issue coming from the Network or Gateway parameters (maximum number of data per hours,....).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 8:27 AM
@STTwo-32 wrote:First the Ping Pong example is a point-to-point application and not a transmission from an End node to network (such as TTN). So, you can't use it for a transmission to a Gateway.
But does that matter?
This is just for EMC testing - so won't just any transmission do?
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 8:44 AM
No, but I've just wanted to clarify more about the Use cases since this post will be visible by other Users that may have confusion between LoRa and LoRaWAN use cases.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-04 12:58 AM
Hi @STTwo-32
Thanks for the clarification.
For the ping pong scenario to be used, the test house needs the two devices to be on fixed channels. For example device 1 will be fixed on channel 1 and device 2 will be fixed on channel 8.
How can this be configured?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-24 10:07 AM
Could you clarify more. Channels is on the concept of LoRaWAN not on Ping Pong.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.