cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I'm trying to enable the Bootloader Mode on my STM32WB55. I succeeded in doing so and the DFU in FS mode is shown in the device manager.I downloaded the DfuSe Demo application and there is nothing in the available DFU Devices section. any help? thanks

WYous.1
Associate III
 
1 REPLY 1
Remy ISSALYS
ST Employee

Hello,

DFU demo application is now deprecated and replaced by STM32CubeProgrammer. You can try to use it and if problem persists, you can check either boot options (Boot0/1) or HW connection.

Best Regards