2022-05-13 1:53 AM
I have already done it, but I want to change the code for the P-NUCLEO-LRWAN3
gateway. Is it possible to share the code if you have it?
I use the bin file for the gateway and the expansion code for the end-devices.
Board used: https://www.st.com/en/evaluation-tools/p-nucleo-lrwan3.html
2022-05-13 2:32 AM
The Gateway code is closed-source.
You'd have to negotiate with RisingHF about getting source code, or getting changes implemented.
Why do you feel that you need to change the Gateway firmware?
BTW: Please try to keep the topic title to a single line - it makes the forum listing much easier to read ...