2021-08-06 08:34 AM
Hello, I have a problem running any project in STM32CubeIDE v1.7.0
When I press 'Run' I usually get "Launching: Performing pre-launch check..." and it just hangs there.
Sometimes it gets past that, and then I get the following error
Error in final launch sequence: Failed to execute MI command: target remote localhost:61234
Error message from debugger back end: localhost:61234: The system tried to join a drive to a directory on a joined drive.
at org.eclipse.cdt.dsf.mi.service.command.AbstractMIControl$RxThread.processMIOutput(AbstractMIControl.java:1014) at org.eclipse.cdt.dsf.mi.service.command.AbstractMIControl$RxThread.run(AbstractMIControl.java:843)
Console output:
STMicroelectronics ST-LINK GDB server. Version 5.9.1
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
2022-03-22 02:44 AM
I had the same issue with CubeIDE v1.7.0 and this also worked for me. Thnaks
2022-03-22 12:45 PM
This is just a common issue which happens randomly. With a bit of luck, not often. I find it happens more often when running Cube over RDP (remote desktop). Often the solution is to unplug/replug the USB cable into STLINK, close Cube, and terminate the ST process in Windows Task Manager, which is a hassle because you can't unplug the USB cable remotely : - )
2022-06-01 06:27 AM
It seems to me that the solution in the video was to tweak the USB cable
2022-10-18 07:21 PM
Well ... It is 2022 now, perhaps I am late. But just in case someone has the same question and tried removing/changing the USB as suggested in the previous comment, it did not work. So, my board only started to behave in such a manner after I turned on the FreeRTOS and changed the Serial wire to the Trace function. So cut long story short. I used STM32CubeProgrammer and cleared the full chip and upgraded the firmware, after this everything works perfectly.
2022-10-19 09:50 AM
Just find the gdb process that is using the port in question and kill it. Eg. in my case on Linux I do this:
killall ST-LINK_gdbserver
You can likely find the process by doing:
ps -aux | grep gdb
As to why this problem happens or how to prevent it in future, I have no clue.
2024-05-29 09:30 AM
This worked for me .
Thank you so much for the solution 🙂