cancel
Showing results for 
Search instead for 
Did you mean: 

Files missing on wiki page STM32WB_OpenThread_Border_Router_Application

CLeli.1
Associate II

I am trying to familiarise myself with the thread using the wiki page STM32WB_OpenThread_Border_Router_Application and am not getting anywhere because some graphics are missing on the page and I especially need the graphic with the CLI commands. It is the graphic File: Connectivity 1-12-0.png

5 REPLIES 5
STTwo-32
ST Employee

Hello @CLeli.1 

This screenshot is useful only if you are using the STM32CubeWB V1.12.0. For the newest versions, you will not need to use those CLI commands.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello STTwo-32,

with the version command I get this:

version
OT/SHA-1: 4a0d6b7b6495a1e4e2e03ab7a4f8baa064df4a6e; STM32WB V1.3.0 Thread_FTD; Aug 21 2024 18:03:41

Is this the newest version and how can I commission this node to my OpenThread Border Router? Pressing SW1 has no reaction.

Unfortunately, the procedure described with the Thread Commissioning App does not work for me.

Best regards,
Chris

Hello @CLeli.1 

Could you please try the last Version (STM32CubeWB V1.21.0).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello STTwo-32,

Now I compiled Thread_Cli_Cmd out of the last Version (STM32CubeWB V1.21.0) and programmed the stack out of this package and the compiled application. Now the command line is not responding and LED1 to LED3 produce a slowly running light. Pressing SW1 shows no response. 

What do I have to do now to join my Nucleo board into the Thread network?

Best regards,
Chris

Hello @CLeli.1 

Have you followed the recommendations of the Wiki page and the Readme file of the example. If so, it should work fine.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.