2025-01-03 08:30 AM
Hi. I have a problem with the STM32WB09KE board.
I'm trying to activate Bluetooth LE using this developer board but the BLE init function returns this error massage.
Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET
Success: aci_hal_set_tx_power_level command
Success: aci_gatt_srv_profile_init command
Success: aci_gap_init command
Public Bluetooth Address: 00:08:e1:2a:12:34
Success: Gap_profile_set_dev_name - Device Name
Success: Gap_profile_set_appearance - Appearance
Success: aci_gap_set_io_capability command
Fail: aci_gap_set_security_requirements command, result: 0x11
==>> End BLE_Init function
Services and Characteristics creation
Success: aci_gatt_srv_add_service command: WB09KES
End of Services and Characteristics Creation
Is there anyone who knows about this? and How to solve this.
In the code, the input value of aci_gap_set_security_requirements() is below.
I don't think this code is wrong because CubeMX automatically makes it.
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.mitm_mode = CFG_MITM_PROTECTION;
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.encryptionKeySizeMin = CFG_ENCRYPTION_KEY_SIZE_MIN;
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.encryptionKeySizeMax = CFG_ENCRYPTION_KEY_SIZE_MAX;
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.bonding_mode = CFG_BONDING_MODE;
ret = aci_gap_set_security_requirements(bleAppContext.BleApplicationContext_legacy.bleSecurityParam.bonding_mode,
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.mitm_mode,
CFG_SC_SUPPORT,
CFG_KEYPRESS_NOTIFICATION_SUPPORT,
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.encryptionKeySizeMin,
bleAppContext.BleApplicationContext_legacy.bleSecurityParam.encryptionKeySizeMax,
GAP_PAIRING_RESP_NONE);
Solved! Go to Solution.
2025-01-07 02:06 AM
Hello @KKIM.6
The aci_gap_set_security_requirements() command return an error with the code 0x11 that means a BLE_ERROR_UNSUPPORTED_FEATURE if KeyPress_Notification_Support is set to 1 but Secure Connection feature is not supported. Those two parameters are configured throw CubeMX and you can solve it by setting the CFG_BLE_SECURE_CONNECTIONS_ENABLED to Enabled (set by default to Disable on CubeMX):
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-07 02:06 AM
Hello @KKIM.6
The aci_gap_set_security_requirements() command return an error with the code 0x11 that means a BLE_ERROR_UNSUPPORTED_FEATURE if KeyPress_Notification_Support is set to 1 but Secure Connection feature is not supported. Those two parameters are configured throw CubeMX and you can solve it by setting the CFG_BLE_SECURE_CONNECTIONS_ENABLED to Enabled (set by default to Disable on CubeMX):
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-09 09:36 AM
Thanks. The problem has been solved by this modification.