cancel
Showing results for 
Search instead for 
Did you mean: 

Example of low power consumption for B-L072Z-LRWAN1

DuCanard
Associate II

Hello,
I use B-L072Z-LRWAN1 and I would like to know how to use it in very low power consumption. By default on mbed OS 6 with one hand with only one ThisThread::sleep_for(3s) I have a consumption of 10.45mA. I take my measurements with an amperemeter in series with the battery box. According to this post (https://community.st.com/t5/wireless-mcu/excess-current-consumption-running-b-l072z-lrwan1-from-battery/td-p/322961/page/2) to reduce my consumption I removed SB18, R26, D2. For the code I tried this code (https://github.com/janjongboom/stm32-standby-rtc-wakeup/blob/master/stm32_standby.h) which puts me at a consumption of 4.00mA. I'm new to MCUs and I'd like to know how I can reach the uA in the code or by another hardwre modification.
Thanks in advance for your reply

4 REPLIES 4

Sleeping only deals with the MCU. Expect to have to turn off Radio, TCXO, LEDs and anything else attached to the MCU that draws current.

Pull the circuit diagram / schematic, and walk-thru that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DuCanard
Associate II

I've looked into these possibilities
I have looked at the datasheet for the radio module ( https://www.mouser.com/catalog/specsheets/Murata_CMWX1ZZABZ-091.pdf ) and I have no idea how to put the lora card in standby mode.

As for the TCXO, I can't see where I can reduce its frequency.

I think I'm lacking knowledge in this area

Hello @DuCanard and welcome to ST Community.

I suggest you to take a look on this post i think it can be a good start for you.

When your question is answered, please close this topic by choosing "Accept as Solution". This will help other users find that answer faster.

Issam

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

DuCanard
Associate II

Thank you @IIRHO.1 for your reply.
I followed the tutorial and removed the HAL_PWREx_EnableFlashPowerDown(); line, which must not be compatible with my card, and I get 3.4mA at best, which is better, but still a long way from microampere.