cancel
Showing results for 
Search instead for 
Did you mean: 

Error: fwdelete Operation Failure! Please, try again

Ra.1
Associate II

Hello I am using stm32wb55 nucleo i am tring to delete the firmware but it shows error

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD -fwdelete

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.6.0

   -------------------------------------------------------------------

ST-LINK SN : 066CFF303430484257141344

ST-LINK FW : V2J37M26

Board    : P-NUCLEO-WB55

Voltage   : 3.25V

SWD freq  : 4000 KHz

Connect mode: Normal

Reset mode : Software reset

Device ID  : 0x495

Revision ID : Rev Y

Device name : STM32WBxx

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M4

Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

Warning: Option Byte: nboot0, value: 0x1, was not modified.

Warning: Option Byte: nboot1, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Succeeded to set nSWboot0=0 nboot1=1 nboot0=1

Memory Programming ...

Opening and parsing file: 0x495_FUS_Operator.bin

 File     : 0x495_FUS_Operator.bin

 Size     : 11584 Bytes

 Address    : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 2]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:00.401

Application is running

Reconnecting...

Reconnected !

Error: FUS_STATE_ERR_UNKNOWN

Firmware delete n░1 failed after retrying!

Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

Warning: Option Byte: nboot0, value: 0x1, was not modified.

Warning: Option Byte: nboot1, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Succeeded to set nSWboot0=0 nboot1=1 nboot0=1

Memory Programming ...

Opening and parsing file: 0x495_FUS_Operator.bin

 File     : 0x495_FUS_Operator.bin

 Size     : 11584 Bytes

 Address    : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 2]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:00.406

Application is running

Reconnecting...

Reconnected !

Error: FUS_STATE_ERR_UNKNOWN

Firmware delete n░1 failed after retrying!

Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

Warning: Option Byte: nboot0, value: 0x1, was not modified.

Warning: Option Byte: nboot1, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Succeeded to set nSWboot0=0 nboot1=1 nboot0=1

Memory Programming ...

Opening and parsing file: 0x495_FUS_Operator.bin

 File     : 0x495_FUS_Operator.bin

 Size     : 11584 Bytes

 Address    : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 2]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:00.343

Application is running

Reconnecting...

Reconnected !

Error: FUS_STATE_ERR_UNKNOWN

Firmware delete n░1 failed after retrying!

Error: fwdelete Operation Failure! Please, try again

plz give me the solution

36 REPLIES 36
Imen.D
ST Employee

Hello @Ra.1​ and welcome to the Community :)

I recommend you to update the STM32CubeProgrammer and use the latest release V2.8.0 which contains enhancement as support of FUS version display for the STM32WBxx microcontrollers.

Please keep me informed about your update.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Ra.1
Associate II

Hello Imen,

thank you so much for your quick response

As per your suggestion i updated the STM32CubeProgrammer and run it in cmd prompt so get same error..!!

even in software it shows

fus state: fus_idle

fus status : fus_no_error

fus version : v0.0.0.0

0693W00000D2PLPQA3.png 

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD -fwdelete

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.8.0

   -------------------------------------------------------------------

ST-LINK SN : 066CFF303430484257141344

ST-LINK FW : V2J37M26

Board    : P-NUCLEO-WB55

Voltage   : 3.25V

SWD freq  : 4000 KHz

Connect mode: Normal

Reset mode : Software reset

Device ID  : 0x495

Revision ID : Rev Y

Device name : STM32WB5x

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0xd5

Debug in Low Power mode enabled

Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

Warning: Option Byte: nboot0, value: 0x1, was not modified.

Warning: Option Byte: nboot1, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Succeeded to set nSWboot0=0 nboot1=1 nboot0=1

Memory Programming ...

Opening and parsing file: 0x495_FUS_Operator.bin

 File     : 0x495_FUS_Operator.bin

 Size     : 8 KBytes

 Address    : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 1]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:00.410

Application is running, Please Hold on...

Reconnecting...

Reconnected !

Error: FUS_STATE_ERR_UNKNOWN

Firmware delete n░1 failed after retrying!

Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

Warning: Option Byte: nboot0, value: 0x1, was not modified.

Warning: Option Byte: nboot1, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Succeeded to set nSWboot0=0 nboot1=1 nboot0=1

Memory Programming ...

Opening and parsing file: 0x495_FUS_Operator.bin

 File     : 0x495_FUS_Operator.bin

 Size     : 8 KBytes

 Address    : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 1]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:00.332

Application is running, Please Hold on...

Reconnecting...

Reconnected !

Error: FUS_STATE_ERR_UNKNOWN

Firmware delete n░1 failed after retrying!

Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

Warning: Option Byte: nboot0, value: 0x1, was not modified.

Warning: Option Byte: nboot1, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Succeeded to set nSWboot0=0 nboot1=1 nboot0=1

Memory Programming ...

Opening and parsing file: 0x495_FUS_Operator.bin

 File     : 0x495_FUS_Operator.bin

 Size     : 8 KBytes

 Address    : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 1]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:00.368

Application is running, Please Hold on...

Reconnecting...

Reconnected !

Error: FUS_STATE_ERR_UNKNOWN

Firmware delete n░1 failed after retrying!

Error: fwdelete Operation Failure! Please, try again

Imen.D
ST Employee

Did you try "connect under reset"?

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Ra.1
Associate II

yes...like by keep pressing reset button after connecting usb need to release the button right..??

i tried like that

Ra.1
Associate II

here board is connecting proprly its detecting in STM32CubeProgrammer tool and cubeIDE so i can upload the example program also..so no connection issue

the problem is not possible to delete the firmware

Ra.1
Associate II

Hi imen,

still no response....!!!

i think its waste community compared to Devzone(nordic) or E2E(TI)

Ra.1
Associate II

Any way we planned to change the controller for our project Due to your poor support

Imen.D
ST Employee

Hello @Ra.1​ 

I apologize for the delay I sometimes take to answer , as I'm busy this period.

I will escalate this issue internally for analyze.

Hi @Houda GHABRI​ , @Remi QUINTIN​ 

Can you please help on this post ? What can be the root cause of such issue.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Remi QUINTIN
ST Employee

Could you download all the option bytes?

How old is your Nucleo board?