2022-02-14 4:03 AM
2022-02-14 4:41 AM
The STM32WLE contains a licensed IP from Semtech, but no SX126x. The reference manual RM0453 RM0461 (see below) lists all the features of the contained LoRa® part.
Regards
/Peter
2022-02-14 5:01 AM
The implementation is done on a single die, rather than a stacked die using a discreet SX126x.
The connection is via an internally routed SPI.
The register set/programming for LoRa should be materially the same as for an SX1262
2023-03-21 1:06 AM
Hello @Peter BENSCH I think the reference manual for the STM32WLE is RM0461.
The RM0453 you mention is for the SMT32WL family.
2023-03-21 1:11 AM
Thank you for pointing that out, I had actually mixed it up by mistake. Yes, RM0461 is the correct reference manual for the STM32WLE.
Regards
/Peter
2023-03-21 1:19 AM
The linked document indicates it was from Jan 2023, so is going to be different to the one Peter posted originally in Feb 2022
I would agree with that this March 2023 document for the STM32WLEx is currently more appropriate.
Document still does state which Semtech IP it is modelled after.
2023-03-21 1:29 AM
You are welcome. If you have experience with the STM32WLE, please take a look at my problem STM32WLE5 'Failure To Execute Command' - I read the reference manual and search the forum, but I can't find an answer to this..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.