cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STM32WB55RG micro controller chip offer inbuilt WiFi module?

JSing.7
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

As also mentioned on the STM32WB55RG website, the device contains a Cortex-M4 for user applications and is equipped with a 2.4GHz radio and the corresponding Cortex-M0, which can cover BLE 5.3, 802.15.4, Zigbee, Thread or Matter; WiFi is not included.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

As also mentioned on the STM32WB55RG website, the device contains a Cortex-M4 for user applications and is equipped with a 2.4GHz radio and the corresponding Cortex-M0, which can cover BLE 5.3, 802.15.4, Zigbee, Thread or Matter; WiFi is not included.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.