cancel
Showing results for 
Search instead for 
Did you mean: 

USBC PD TCPM on the STM32U5

rward
Associate

Hello,

I have an application that uses the TCPM/TCPC architecture, with a STM32U5 acting as the port manager, and the FUSB307B as the port controller. I want to use the USB-PD middleware stack for the policy engine, however, when looking at the available libraries, there is no USBPDTCPM_PD3_FULL_xxxx.a for the Cortex-M33. Are there any compatible TCPM libraries for the STM32U5? I do not want to use the inbuilt USBPD PHY, and only want/need to use the policy engine and port managing capabilities of the USB-PD library.

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hello @rward and welcome to ST community,

Unfortunately, TCPM stack should be no longer supported for newer products. As a workaround, you can use the CM0 version of the lib (a library compiled for CM0 will be able to run on CM33, the opposite is not possible) X-CUBE-USB-PD - USB Type-C and Power Delivery software expansion for STM32Cube (UM2073) - STMicroelectronics

Would you please specify the number of ports required? Why not using U5 internal port? If you need 2 ports, you can use STM32G0. It embeds 2 ports type C.

I hope this helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

1 REPLY 1
FBL
ST Employee

Hello @rward and welcome to ST community,

Unfortunately, TCPM stack should be no longer supported for newer products. As a workaround, you can use the CM0 version of the lib (a library compiled for CM0 will be able to run on CM33, the opposite is not possible) X-CUBE-USB-PD - USB Type-C and Power Delivery software expansion for STM32Cube (UM2073) - STMicroelectronics

Would you please specify the number of ports required? Why not using U5 internal port? If you need 2 ports, you can use STM32G0. It embeds 2 ports type C.

I hope this helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL