2021-08-30 7:20 AM
I'm working on a mobile project based on the STM32WB5MMG.
First, we bought a P-NUCLEO-WB55 and had a look at some of the example projects.
After a good experience with the Nucleo board, we decided to build HW around the controller.
Now the HW is working and the BLE_Stack has been flashed to the device.
Even some examples are working on our platform.
Now I want to implement two specified services "Battery Level" and "Automation I/O".
For this, I build upon the "BLE_Custom" example and moved to a custom .ioc file/project later.
But now I'm stuck. Is there any documentation of the generated code for the "Custom Template"? I found a few functions in the STM32WB HAL library, but non of the template-related stuff.
Detailed Problems:
1) I'm able to show services and characteristics to a device (phone/pc) read and write to it.
Now, I would like to update a specific characteristic. Therefore I used "aci_gatt_update_char_value()". But it seems I'm, not allowed to change the value while the service is running.
2) I would like to notify a client of new data. Therefore I tried to implement the "Hear Rate Measurement" from the "BLE_Custom" template. In the code I get the "CUSTOM_STM_HRS_M_NOTIFY_ENABLED_EVT", but how can I change the value and notify the client?
2021-10-26 6:17 AM
Hello,
Could you please provide us with the software's versions that you are using ( STM32CubeMX, Firmware, IDE..)
Best Regards,
Sara