2024-01-20 01:23 PM - last edited on 2024-01-22 01:02 AM by STTwo-32
Hello,
I followed the indtructions from here, https://www.youtube.com/watch?v=vuc6914B0KM and I setup the NUCLEO-WL55JC STM32WL Nucleo-64 board and sensor board X-NUCLEO-IKS01A3 with LoRaWAN Gateway P-NUCLEO-LRWAN2 through The Things Network (TTN).
In this moment I am able to see the raw data in TTN Live data watch.
In the youtube 5 video example, the autor use the Cayenne app to create dashboard in order to decode and siaplay the sensor data.
Now, the issue is this: Cayenne is no more available, could you provide a Decoder code in JSON format for uplink and downlink, for application example LoRaWAN_End_Node?
Thank you,
Mihai
2024-09-25 05:57 AM
Hello @MihaiMEC
No need for a modification on the Code of the LoRaWAN_End_Node. You can keep using the DATACAKE for example or the Zafron platform that can receive the same data frame as on Cayenne.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.