2026-02-03 8:28 AM - last edited on 2026-02-27 1:29 AM by Imen.D
Code is written using stm32CubeMX. Connecting with stmlink V3 Minie.
Executing step by step, it appears that debug fails (lose connection) when executing debug_init. In fact debug_init creates the problem when programming pa13.
When removing the initialization of PA13 and PA14 in debug init, things seems to work but I have no idea of potential side effect.
An recommendation?
Solved! Go to Solution.
2026-02-05 10:15 AM
@GYV wrote:What is the appropriate way to initialise this macro?
You need to do it somewhere in the C source code
#define CFG_DEBUGGER_SUPPORTED 1
2026-02-03 8:38 AM
Please include the IOC that generates the problematic code.
2026-02-03 8:39 AM - edited 2026-02-03 8:40 AM
Welcome to the forum.
Please see How to write your question to maximize your chances to find a solution for best results.
In particular, please give details of your setup.
@GYV wrote:debug fails (lose connection) when executing debug_init. In fact debug_init creates the problem when programming pa13.
Please show that code. See: How to insert source code
PA13 & PA14 carry the SWD signals (ie, the signals the debugger uses to communicate) - so messing with them will break the debugger connection!
https://www.st.com/resource/en/datasheet/stm32wb55rg.pdf#page=65
via: https://www.st.com/en/microcontrollers-microprocessors/stm32wb55rg.html#documentation
2026-02-04 10:26 AM
2026-02-04 10:31 AM
Sorry my english fails me here. What "IOC" stands for, or what additional info do you need?
Thanks
2026-02-04 10:40 AM
Set CFG_DEBUGGER_SUPPORTED = 1 to enable debug support. If this is 0, debug support is disabled and the pins are reconfigured to analog, as you can see in the code.
IOC is the file type of an STM32CubeMX project.
2026-02-05 10:05 AM - last edited on 2026-02-05 10:14 AM by Andrew Neil
Hello, after your message I look the code one more time and I think you are correct.
My IOC file (see attched) does not contain reference to CFG_DEBUGGER_SUPPORTED .
I tried adding CFG_DEBUGGER_SUPPORTED=1 as the last line of the IOC file (using notepad). I re-open CubeMX and generate the code. Closed CubeMX and reopen IOC file with notepad and noticed that the line i added (i.e. CFG_DEBUGGER_SUPPORTED=1) did not exist anymore.
Looking at the generated code (specifically a #if (CFG_DEBUGGER_SUPPORTED ==1)) is grayed out confirming that the macro is not initialized.
What is the appropriate way to initialise this macro?
Thanks
2026-02-05 10:15 AM
@GYV wrote:What is the appropriate way to initialise this macro?
You need to do it somewhere in the C source code
#define CFG_DEBUGGER_SUPPORTED 1
2026-02-07 12:56 AM
I added one statement to avoid compiler warning:
#undef CFG_DEBUGGER_SUPPORTED
#define CFG_DEBUGGER_SUPPORTED 1
:
2026-02-09 2:10 AM
@GYV wrote:I added one statement to avoid compiler warning
Presumably, that warning was telling you that it was already defined?
Then it would also have told you where that original definition was - so you could have edited the original definition ...