cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMonitor-RF - How to change TX Interval for RF-Tests?

Cubenator
Associate

Hello

I am able to succesfully run the "RF Tests" using a nucleo board (STM32WB55) and a dongle, both connected on the same computer via virtual com port.

Now I'd like to change some parameters for the test, e.g. the TX interval on the nucleo board.

I thought I can do this via the ACI commands HCI_LE_SET_ADVERTISING_PARAMETERS.

However, if I change the minimum and maximum advertising interval, nothing changes. I run the test for about 5s and I get about 8000 packets on the receiver which corresponds to the 0.625 ms interval. If I change the intervals, I still get 8000 packets.

What do I am missing here?

1 REPLY 1
Remy ISSALYS
ST Employee

Hello,

Can you tell us which command sequence are you using and how you count the packets?

Best Regards