2021-06-09 5:17 PM
Hi,
I have P-NUCLEO-LRWAN2 starter pack and I'm trying to run AT Master application on NUCLEO-LRWAN1/NUCLEO-L073RZ pair with supplied in I-CUBE-LRWAN Expansion Package. It looks like all fine (i.e firmware compiled and loaded onto NUCLEO-L073RZ without any problem). But GW cant get any data from the Sensor Device. Finally, when I checked with SDR , I cant see any Tx activity from the Sensor device .. I will be so happy if you can make comment on this. many thanks in advance, reha
2021-07-13 3:06 AM
@Shati.1 "the L073RZ with the expansion do not work with tera term"
It's not intended to work with TeraTerm (or any other terminal) - it is a standalone node.
This is described in the P-NUCLEO-LORWAN2 documentation.
Cross-post:
2021-07-13 3:08 AM
@ZAHİDE ZEYNEP KURT "I need to buy this device"
Which device?
For the LoRa node, I would suggest that you get the B-L072Z-LRWAN1 Discovery board
2021-07-13 5:14 AM
P-NUCLEO-LRWAN1 What is the difference between P- and NUCLEO-LRWAN3? why did you recommend P-NUCLEO-LRWAN3? My goal is to have a lora in the center. and the communication of the surrounding lora with the central lora. but i don't know how to do
2021-07-13 6:32 AM
Hi,
1) WAN1 is 868Mhz and WAN3 is 433MHz..
2) GW HW is the same
3) LORA Module on Device is different..
But in practice they are very similar. thanks
2021-07-13 8:17 AM
The "P-" prefix refers to a "Pack"
The User Manual tells you the difference between the P-NUCLEO-LRWAN2 and P-NUCLEO-LRWAN2 packs:
2021-07-14 3:04 AM
Hi, i m working now with the B-L072Z-LRWAN , and it's work good. but i want to read data from an externel sensor . please how can i read data from a sensor and send it with lora .
2021-07-14 3:27 AM
Hi Shati,
please notice that this topic is for NUCLEO-LRWAN1/NUCLEO-L073RZ pair not for B-L072Z-LRWAN
2021-07-14 4:43 AM
Yes. @Shati.1 - start a new topic (thread) on that.
Give a link here to your new thread;
In the new thread, give a link to this one for background.
EDIT
Oh, you already have started a new thread: