2022-11-09 5:22 AM
2022-11-10 9:14 AM
Hello,
The semaphore 4 (CFG_HW_ENTRY_STOP_MODE_SEMID) is released in ExitLowPower function in every case and in some circumstances the semaphore is released earlier in EnterLowPower. The algorithm to enter and exit stop mode on CPU1 are describes in AN5289 (see figure 6 and 7).
Best Regards
2022-11-11 9:16 AM
Hi Remy,
Thanks for answering that. It would be good if that was documented in the code to prevent me asking :)