2021-04-12 8:27 AM
I tested BLE example with NUCLEO-WB55 board. It worked well.
Now we are going to run the BLE example on the custom board.
I made a board with STM32WB55CE MCU.
Although the custom board application was uploaded as shown in the example NUCLEO-WB55, an error occurs in the code shown below.
app_ble.c
/**
* Starts the BLE Stack on CPU2
*/
if (SHCI_C2_BLE_Init( &ble_init_cmd_packet ) != SHCI_Success)
{
Error_Handler();
}I thought the BLE stack went up wrong, so I uploaded the BLE stack, but it doesn't work the same way.
Where should I look?
2021-12-06 10:12 AM
Did you ever find a solution for this? I'm experiencing the same issue
2021-12-09 8:31 AM
I'm seeing the same issue with our custom board with a STM32WB55CE MCU. I assume no solution has been found?
2021-12-13 2:58 PM
Having the same issue here with the Thread stack: the program hangs at "ThreadInitStatus = SHCI_C2_THREAD_Init();"
I am running the exact same code as I did on the Nucleo board with the exact same option bytes and FUS version. Only difference is that I am using a custom board now.
Did you ever figure out a solution for this?
2021-12-14 5:48 AM
Unfortunately not. I thought I had fixed one of the boards by upgrading the BLE firmware from 1.12.1 to 1.13.0 but when I tried to repeat that fix on another board I keep getting the FUS_STATE_IMG_NOT_AUTHENTIC error at the end of the update and the build still fails at SHCI_C2_THREAD_Init().
2021-12-16 12:05 PM
After talking with stm32 for a bit, I scrapped everything, as they sent me this much newer tutorial: https://www.youtube.com/watch?v=i10X4Blr8ns&t=16s
Using this I was able to get things running to the point that the bluetooth micro was spitting out:
“Wireless Firmware version 0.0.0
Wireless Firmware build 0
FUS version 1.1.1
SHCI_SUB_EVT_CODE_READY - FUS_FW_RUNNING�?
At that point, it was pointed out that while my FUS was fine, I needed to upgrade my wireless stack.
After doing that everything worked cleanly.
Good luck.
2022-03-12 8:23 AM
Was anyone on this post able to figure out what solves this issue? I am having the same problem but with the Zigbee stack, the function call SHCI_C2_ZIGBEE_Init() never returns.