Bare metal SPI implementation problem
- April 14, 2025
- 11 replies
- 1238 views
Hi,
I'm trying to get a bare metal implementation of SPI working on a STM32WB55 Nucleo board.
The transmit appears to work but I cant get the receive function to work. I'm using a loop back by connecting MOSI & MISO with a jumper.
When in debug I can see my Tx buffer getting loaded with the appropriate value but it never appears in the Rx buffer. When I step through the Tx code runs through as expected, in the Rx code though it looks like the SPI_FLAG_RXNE never gets set i.e. nothing ever arrives.
Ultimately I'm trying to connect with 2 x ADXL362s over the SPI bus.
I have attached a zip of the CubeIDE.
Any help with debugging this or pointers to how I go about that would be most appreciated. I'm getting code blindness trying to find the problem.