2020-08-24 7:27 PM
Hi
I am trying to generate a true random number on the B-LO72Z-LRWAN1 using the HAL_RNG_GenerateRandomNumber function with the code below:
uint32_t rnd_generator (void) {
RNG_HandleTypeDef RngHandle; // RNG handler declaration
uint32_t rv;
RngHandle.Instance = RNG;
if (HAL_RNG_Init(&RngHandle) != HAL_OK) {
printf ("\n Error RNG_Init \n");
}
if (HAL_RNG_GenerateRandomNumber(&RngHandle, &rv) != HAL_OK) {
printf ("\n Error RNG_Generate \n");
}
HAL_RNG_DeInit(&RngHandle);
return rv;
}
The HAL_RNG_GenerateRandomNumber always returns an error and the generated number is always the same.
I believe that I must initialize the clock for the RND module using my own version of the HAL_RNG_MspInit and HAL_RNG_MspDeInit functions.
Can you provide me some help on this?
BR
Gilberto
2020-08-24 7:44 PM
STM32Cube_FW_L0_V1.11.0\Projects\NUCLEO-L073RZ\Examples\RNG\RNG_MultiRNG\Src\stm32l0xx_hal_msp.c
/**
* @brief RNG MSP Initialization
* This function configures the hardware resources used in this example:
* - Peripheral's clock enable
* @param hrng: RNG handle pointer
* @retval None
*/
void HAL_RNG_MspInit(RNG_HandleTypeDef *hrng)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/* Enable HSI48 Oscillator for USB/RNG */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
/* Initialization Error */
while(1);
}
/* configure RNG clock for USB or RNG analog part */
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
if(HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct)!= HAL_OK)
{
/* Initialization Error */
while(1);
}
/* RNG Peripheral clock enable */
__HAL_RCC_RNG_CLK_ENABLE();
}
/**
* @brief RNG MSP De-Initialization
* This function freeze the hardware resources used in this example:
* - Disable the Peripheral's clock
* @param hrng: RNG handle pointer
* @retval None
*/
void HAL_RNG_MspDeInit(RNG_HandleTypeDef *hrng)
{
/* Enable RNG reset state */
__HAL_RCC_RNG_FORCE_RESET();
/* Release RNG from reset state */
__HAL_RCC_RNG_RELEASE_RESET();
}