2021-03-30 05:23 AM
I am using B-L072Z-LRWAN1. I ran the ping pong application ready here. I wanted to set up timer interrupt myself but there is no .ioc file. I opened another project, set up a timer in cubemx, tried and run it, and added it to the ping pong project. but timer interrupt ping pong did not work in the project. I wonder if you have a solution.
2021-03-30 08:48 AM
The code was written by an engineer, not code-generated, and based on Semtech's model, not ST's
Add the TIM code as if you were using the HAL directly.
Look at the HAL TIM examples
2021-03-30 11:05 PM
hello I just added the state code but I couldn't run it. I wonder if I'm trying to use a timer that I shouldn't use. I used timer 2-3-4. I am working for my university project. I will be glad if you help.
2021-03-30 11:05 PM
hello I just added the state code but I couldn't run it. I wonder if I'm trying to use a timer that I shouldn't use. I used timer 2-3-4. I am working for my university project. I will be glad if you help.