Are .bin outputs byte-aligned for the boards flash size?
Board: STM32WB55
Software: STM32CubeIDE
Background: I am experimenting with a Custom Bootloader to enable USB and BLE updates to my firmware. I'm getting the IDE to export .bin and .hex files on build, so I can pass my main application into the bootloader by an application to replace the current main application stored in Flash memory. The STM32WB55 needs to write to on-board Flash with a 64-bit Double Word (8 Bytes).
Issue: Is the .bin file that is created by the IDE aligned to this size? Is there a way to ensure that? I do not know if simply padding the end of the .bin file with 0's to make the last 8 bytes / padding each .hex line as needed with 0s is a safe (and memory efficient!) option? I am relatively fresh to this area.
Any advice much appreciated,
Thank you