2020-08-25 07:28 PM
I try to create a graphic application based on stm32h747xi. When I tried to select x-cube-touchgfx in stm32cubemx. the option is gray and a warning says "this pac cannot be used on the selected MCU". Does stm32h747xi really not support x-cube-touchgfx.4.14.0
Solved! Go to Solution.
2020-08-27 01:56 AM
Hi @sliu.2 ,
I am sorry, but I can not help you with this. I have been trying to integrate TouchGFX project with Cube project for while (for STM32H747i-DISCO), but with no success. You could try to make TouchGFX project for STM32H743 and try to make integration manually by the template (copy neccessary files). I was trying to make it this way, but still with no success. As I said I "solved" it by purchasing STM32F769i-DISCO, because I did not want to wait for adding support for dual core.
Best regards
Jan
2020-08-26 12:42 AM
Hi,
you are right, because x-cube does not support multicore devices like STM32H747i-DISCO. I have met the same problem (solved by purchasing STM32F769i-DISCO) for now.
But I saw the post on this forum about adding multicore support in Q4 2020.
Best regards
Jan
2020-08-26 02:34 AM
Hello @sliu.2
Thanks for the feedback, it's not an issue but for the Dual core, it still not supported, it will be available as soon as possible .
Best regards,
Nesrine
2020-08-26 06:33 PM
Hello @Nesrine.JLASSI
Thanks for your reply. Now that TouchGFX does not support dual core, How can I build graphic application on STM32H747XI? Anyway I have found a TouchGFX folder in the STM32H747I-DISCO_demo project which is downloaded from ST website.
Best regards,
Scliu
2020-08-26 10:50 PM
Hi,
if you want only to build graphics application, you can download x-cube-touchgfx and in folder utilities is installation file of standalone application TouchGFXDesigner.
Best regards
Jan
2020-08-26 11:52 PM
Hello @Jan Pe�?a
Thanks for your reply.
I have a standalone TouchGFX Designer installed as you stated. Then I created a TouchGFX project with no Application Template and UI Template. Also I have created a CubeMX project with STM32H747XI. What do I have to do to integrate the TouchGFX project with the CubeMX project?
Best regards,
Scliu
2020-08-27 01:56 AM
Hi @sliu.2 ,
I am sorry, but I can not help you with this. I have been trying to integrate TouchGFX project with Cube project for while (for STM32H747i-DISCO), but with no success. You could try to make TouchGFX project for STM32H743 and try to make integration manually by the template (copy neccessary files). I was trying to make it this way, but still with no success. As I said I "solved" it by purchasing STM32F769i-DISCO, because I did not want to wait for adding support for dual core.
Best regards
Jan
2020-08-27 02:17 AM
Hello @Jan Pe�?a
I see. Thank you very much.
Best regards,
Scliu
2021-01-07 06:42 AM
Hello,
I am also trying to do a custom project using cubeMX and TouchGFX and I am facing the same problem that it is not compatible yet. In the version Touch GFX Generator v4.16.0 release notes it is specified : "TouchGFX Generator was previously available for projects with dual Core MCUs H747* and H745* despite not being supported yet." Do you have any updates on when it is going to be supported as I saw in this forum that is is planed for Q4 2020.
Thank you for your answer
Best regards
Augustin
2021-01-08 12:38 AM
Hi,
With the release of CubeMX 6.1 we are now currently working on having TouchGFX Generator available for dual cores . I unfortunately cannot give a delivery date yet.
/Romain