TouchGFX 4.24.0 is now out.
Please follow this link to download it.
4.24.0 Release details:
-
Release date: June 6th, 2024
-
New TouchGFX Designer Features:
- Added a QR Code widget.
- Added RGB Compression for images.
-
New TouchGFX Core Features:
- Added RGB Image Compression for 16bpp, 24bpp and 32bpp framebuffer
formats.
-
Bugfixes in TouchGFX Designer:
- Fixed a bug where small screens were not able to display the language
settings properly.
- Fixed a bug where copying and pasting widgets from one screen to another
would invert the order of the widgets.
- Fixed a bug where a user was able to modify the canvas while being in a
different tab, by copying and pasting widgets selected on the canvas.
- Fixed a bug where the user was unable to edit the name of a widget with
the F2 key while being placed inside a container.
- Fixed TextureMapper not showing an image when copying and pasting a
TextureMapper.
- Fixed the text in Log View being editable.
- Fixed erroneous default value behavior for Shade Alpha in ModalWindow.
- Fixed toggling Framework features not signaling outdated code or unsaved
changes.
- Fixed a bug when importing custom containers where certain zipped
archives would cause a crash.
- Fixed changing simulator skin not showing outdated code or unsaved
changes.
-
Bugfixes in TouchGFX Core:
- Removed warning in image converter of unsupported 'viewBox' attribute in
SVGs. For more information please read the article about SVG.
- Vector fonts and SVGs now also work for rotated displays on GPU2D
(NeoChrom) targets.
-
Bugfixes in TouchGFX Core:
- Removed warning in image converter of unsupported 'viewBox' attribute in
SVGs. For more information please read the article about SVG.
- Vector fonts and SVGs now also work for rotated displays on GPU2D
(NeoChrom) targets.
-
Deprecated TouchGFX Core Features:
- Removed types from Types.hpp:
- FrameBuffer::FB_PRIMARY
- FrameBuffer::FB_SECONDARY
- FrameBuffer::FB_TERTIARY
- Gradient::GRADIENT_HORIZONTAL
- Gradient::GRADIENT_VERTICAL
4.23.2 Release details:
Feel free to learn more about our new features by looking into our documentation !
Note : TouchGFX Designer 4.24.0 MUST be used with STM32CubeMX 6.11.0 or above (link to download STM32CubeMX).
Attention : If X-CUBE-TOUCHGFX 4.24.0 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-24-0.zip file to install the new pack inside STM32CubeMX.
Please also check our Known Issues article.
Enjoy this new version ! 🙂
Louis BOUDO
ST Software Developer | TouchGFX