X-CUBE-TouchGFX 4.21.2 is out !
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-06 12:59 AM
TouchGFX 4.21.2 is now out.
Please follow this link to download it.
4.21.2 Release details :
- Release date: March 1st, 2023
- Bugfixes in TouchGFX Designer:
- Fixed crash related to interactions.
- Fixed crash related to deleting texts in search results.
- Fixed SVG picker showing duplicates when undoing selected SVG.
- Fixed physical button names not being visible in interactions.
- Fixed erroneous code generation for Dynamic/Static Graph widget.
- Fixed faulty memory usage related to texts.
4.21.1 Release details :
- Release date: January 16th, 2023
- Bugfixes in TouchGFX Designer:
- Fixed bug where locking a widget would cause it to appear in position (0,0) when compiling the code
- Fixed faulty memory usage when switching between screens
- Fixed case where importing a Custom Container containing a font already existing in the project could cause a crash
- Fixed a case where some widgets would not show their used images correctly when copy/pasted
- Bugfixes in TouchGFX Core:
- Solid colors in SVGs would wrongly be placed in RAM.
4.21.0 Release details :
- Release date: December 19th, 2022
- New TouchGFX Designer Features:
- TouchGFX Stock added. Free designs, images and icons provided within TouchGFX Designer.
- Access to material icons made by Google.
- New SVG Image widget.
- New image picker for all image-related widgets.
- New preset picker for browsing themes and presets.
- Mouse coordinates shown when hovering canvas.
- New action for setting border color on box with border widget.
- Now able to navigate widget menu using arrow keys.
- Progress indicator widgets now support two new triggers, ValueUpdated and ValueUpdatedCompleted.
- Ability to close current project from file menu.
- Designer now remembers start up and save folder.
- Added tooltips for visibility and lock buttons in tree view of canvas.
- Added new icon for lock button in tree view of canvas, to make it more clear if a widget is locked or unlocked.
- Added delay property to move and fade actions.
- Bugfixes in TouchGFX Designer:
- Fixed bug regarding DPI of images used in Analog clock.
- Fixed bugs regarding linespacing.
- Fixed bug with minimum and maximum check for x-range in Static Graph.
- Fixed bug regarding auto-size in TextArea widget.
- Fixed being able to set negative border width on box with border widget.
- Fixed disappearing interaction when undoing.
- Fixed bug with DPI in images used by Gauge widget.
- Fixed bug with not showing an error when deleting wildcard character in TextProgress and DigitalClock widgets.
- Fixed bug with long names in interactions.
- Fixed bug with escaped characters in text.
- Changing startup screen now results in unsaved changes.
- Fixed bug with code generation regarding ScreenAnimationEnded trigger.
- Fixed bug happening when users attempt to open a project with an unknown version.
- Text field size in Widget tree view increased.
- Fixed the ability to select multiple screens using right mouse click.
- Fixed being able to set radius of a Circle Widget to a negative number
- Fixed text for checkboxes not wrapping.
- Fixed image icon not updating when changing simulator skin image.
- New TouchGFX Core Features:
- New widget: SVG Image
- Support in image converter to read basic SVG images. These are converted to binary data that can be drawn using the SVG Image widget. See the documentation for more information.
- New wide text actions and redefinition of two existing formats:
- WIDE_TEXT_NONE: No change, no automatic line breaks.
- WIDE_TEXT_CHARWRAP_DOUBLE_ELLIPSIS: No change, will add two ellipsis at end of the last line in the TextArea.
- ImageConvert is using updated libpng 1.6.38. Generated images look the same.
- WIDE_TEXT_WORDWRAP: Changed, will keep adding line breaks and will not add ellipsis.
- WIDE_TEXT_WORDWRAP_ELLIPSIS: New, will add ellipsis as late as possible (even mid-word) on the last line in the TextArea.
- WIDE_TEXT_WORDWRAP_ELLIPSIS_AFTER_SPACE: No change, automatic line breaks, ellipsis will not be in the middle of a word.
- WIDE_TEXT_CHARWRAP: Changed, will keep adding line breaks and will not add allipsis.
- WIDE_TEXT_CHARWRAP_ELLIPSIS: New, will add ellipsis at end of last line in the TextArea.
- AbstractShape::setFillingRule() added to also allow EVEN-ODD filling, in addition to the default NON-ZERO filling.
- As images on monochrome displays do not support alpha channel, any alpha value is now applied to each pixel before converting to BW.
- Optimized SlideTransition and CoverTransition.
- Class FullSolidRect has been removed from WipeTransition.
- WIDE_TEXT_CHARWRAP_DOUBLE_ELLIPSIS: No change, will add two ellipsis at end of the last line in the TextArea.
- Bugfixes in TouchGFX Core:
- Font metrics are handled better so now font height does not depend on which letters are actually being used. This means that default line spacing might be different - this can be adjusted using TextArea::setLinespacing(). For GraphLabels and ButtonWithLabel, texts might be placed better, depending on your font.
- Setting a negative radius on a Circle will set the radius to zero.
- Setting a negative line width on a Circle will set the line width to zero (causing a filled circle to be drawn).
- More robust handling of timer widgets in cases with lots of timer widgets.
- Fixed performance issue observed when upgrading to TouchGFX 4.19.0, 4.19.1, 4.20.0 (Removed Container::invalidateContent())​
- Font::getSpacingAbove() return type changed from uint8_t to int16_t to prevent overflow.
- Deprecated TouchGFX Core Features:
- Font::getMaxTextHeight() and Font::getMinimumTextHeight() have been replaced by Font::getHeight(). Returns the height of the font.
- Font::getFontHeight() has been replaced by Font::getBaseline(). Returns the distance to the baseline.
Attention : TouchGFX Designer 4.21.0 MUST be used with STM32CubeMX 6.7.0 or above (link to download STM32CubeMX 6.7.0)
Hope you will enjoy this new version !
ST Software Developer | TouchGFX
- Labels:
-
STM32CubeMX
-
TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-06 9:27 AM
I downloaded TOUCHGFX 4.21.2 version and noticed that if I change something in one file it recompiles all project. Does it really needed?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-06 10:08 PM
Hi,
What files are you talking about for example ? Just to have a better context.
/Romain​
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-06 10:14 PM
I'm talking about files which touchgfx generates.(view, presenter files)