cancel
Showing results for 
Search instead for 
Did you mean: 

Why does TouchGFX program need to be manually run in Keil ?

weixun
Associate III

Hi everyone, after I've configured TouchGFX, the program needs to be manually run in Keil's debug environment to execute. Why is that?

My ICNA3306_DrawBlock data transfer did not use DMA.

 

weixun_0-1744464547350.pngweixun_1-1744464566815.pngweixun_2-1744464581182.pngweixun_3-1744464593753.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
weixun
Associate III

I found the problem — the TouchGFX project generated by CubeMX doesn't run when targeting Keil, but it works if it's generated as an STM32CubeIDE project.

View solution in original post

16 REPLIES 16
Andrew Neil
Super User

Welcome to the forum.

For best results, please see: How to write your question to maximize your chances to find a solution;

And, in particular: How to insert source code.

 


@weixun wrote:

the program needs to be manually run in Keil's debug environment to execute.


Not sure what you mean by that?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
GaetanGodart
ST Employee

Hello @weixun ,

 

If you cannot "flash" your program through Keil but you are able to debug it through Keil, try to flash it using STM32CubeProgrammer.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Hi GaetanGodart, thanks for your reply. I am able to flash the chip using Keil. The problem is that the program doesn't run automatically after flashing. I need to start a debug session ('Start/Stop Debug Session') and click 'Step' or 'Step Out' to get it running. I've observed that after stepping out several times, the ICNA3306_Init function is called, but then the execution gets permanently stuck right here:

if (OSWrappers::isVSyncAvailable())
{
    hal.backPorchExited();
}
Is it that I didn't write my OSWrappers::signalVsync correctly?
weixun_0-1744638126362.pngweixun_1-1744638130091.png

 

Hi Andrew Neil, this means 'I need to start a debug session ('Start/Stop Debug Session') and click 'Step' or 'Step Out' to get it running.Sorry, my English isn't very good, so I used a translator.


@weixun wrote:

I am able to flash the chip using Keil. The problem is that the program doesn't run automatically after flashing.


I think you have to configure  that?

Maybe in the Debug settings - configure it to do a download at the start of a session?

Have you got it to work with a simple "Blinky" project?

For questions specifically about the Keil tools, probably best to ask in Keil's own forum:

https://community.arm.com/support-forums/f/keil-forum/

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
weixun
Associate III

I have already uploaded the code to https://github.com/weixuna/touchgfx_amoled_

I don't think it's a Keil issue, because I can flash other programs normally. It's only when I configure TouchGFX in CubeMX that it doesn't work, so it's likely a problem with my code.


@weixun wrote:

 I can flash other programs normally.


But you said you can flash this one OK - it's just a matter of starting the debug session?

Again, I think this is a project setting - presumably, TouchGFX just sets it differently?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hello @weixun ,

 

I have looked at the ICNA3306, it seems it is a third party display that I have no control about. If it's init function is behaving poorly I am not sure I can help with that.

 

You say your program gets stuck and you show a screen shot where the current line is the end of the taskEntry. I have trouble understanding that picture, if you end up on the last line of that function that is just the closing bracket, are you really stuck on this line? There is nothing to get stuck to there.

If you mean that you permanently loop through it (through the if statement), then perhaps you implemented your hal.BackPorchExited() wrongly, you can look at a TBS we made that has a similar configuration as your (same communication, same display type, so RTOS) to see how we implemented it.

 

Regarding your last message to Andrew, maybe you can try to copy the setting file from one of the project that works into your TouchGFX project. I believe it is the "Project.wsdt" file.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)