2025-04-23 3:54 AM
Hi,
what is the best way (excluding asking them to use TouchGFX) to show a preview of a touchGFX project - with just button functionality to navigate between screens - to a someone?
Is there perhaps a viewer for Window or can a project be compiled and sent as .EXE?
If not, what is the best way to send someone an interactive TouchGFX UI project (again, all I need is the navigation between screens through the buttons in the UI)?
Thank you
Solved! Go to Solution.
2025-04-23 6:20 AM
Hello @Ricko ,
You could share the simulator project with them so they can run it on any Windows computer.
To do so, just share the folder build/bin that contains the simulator.exe but also some dll that are required (SDL2, libpng, etc).
Regards,
2025-04-23 6:20 AM
Hello @Ricko ,
You could share the simulator project with them so they can run it on any Windows computer.
To do so, just share the folder build/bin that contains the simulator.exe but also some dll that are required (SDL2, libpng, etc).
Regards,
2025-04-23 6:53 AM
Thank you @GaetanGodart
2025-04-23 7:14 AM
My pleasure! :)