cancel
Showing results for 
Search instead for 
Did you mean: 

Why does TouchGFX 4.13.0 require non-existent STM32CubeMX 5.5.0?

MLang.9
Associate II
  • I downloaded the latest STM32CubeMX v5.4.0
  • Under "Additional Software", TouchGFX v4.13.0 says that it is only compatible with STMCubeMX v5.5.0

Where is STMCubeMX v5.5.0?

...or...

How do I get STM32CubeMX to download a version of TouchGFX that it is compatible with?

Cheers,

Murray

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
Martin KJELDSEN
Chief III

We'll unveil the exact reason for the X-CUBE not being compatible with CubeMX 5.4.0. There's no more TouchGFX Middleware in CubeMX - It's being replaced by "TouchGFX Generator" add-on which now generates your TouchGFX HAL. It feeds the designer input like screen dimensions (=> canvas dimensions) and bitdepth.

/Martin

Jerome B
ST Employee

Hi,

STM32CubeMX 5.5.0 is availble for donwload (https://www.st.com/en/development-tools/stm32cubemx.html) or direct upgrade of your existing install.

Regards

Jérôme

Karl Yamashita
Principal

So this new 5.5.0 shows it is RC6 dated 12-30-2019 and the 5.5.0 that i got from ST support is dated 12-20-2019. They both show an error as shown in the image. I have tried different combinations using the drop downs but i can't get rid of the error which prevents me from generating a project. How do you start TouchGFX from CubeMX? I have both TouchGFX 4.12.3 and 4.13.0 installed. What am i doing wrong?

0690X00000BviFXQAZ.jpg

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

It's not an error. It's a warning to say that you do not need this particular blending factor for your LTDC layer.

Did you read the post i made with links to articles on both installation and use of the generator?

https://community.st.com/s/question/0D50X0000BwjU6pSQE/official-release-xcubetouchgfx-v4130

Could you please create a new post titled with any specific issue you may have? I'm closing this as the question was already answered by Jerome.