cancel
Showing results for 
Search instead for 
Did you mean: 

Which MCU has 3 lane DSI interface

Rostyslav S
Associate II
Posted on October 17, 2017 at 15:58

According to

http://www.st.com/content/ccc/resource/technical/document/application_note/group0/1d/b8/33/4f/dc/0a/45/52/DM00287601/files/DM00287601.pdf/jcr:content/translations/en.DM00287601.pdf

, STM32F4 includes DSI interface with up to 2 lanes. See page 15.

I am wondering if there is any MCU with 3 data lanes (L0, L1, L2) and CLK lane?

#stm32f4 #dsi
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on October 17, 2017 at 17:08

Hi

rostokus

,

Unfortunately,there is no STM32 device with 3 DSI data lanes, the STM32 embeded maximum 2 data lanes.

-Nesrine-

View solution in original post

3 REPLIES 3
Nesrine M_O
Lead II

Posted on October 17, 2017 at 16:16

 Hi rostokus,

The STM32F469/479 devices embeded MIPI® DSI host controller supporting up to 720p 30Hz resolution.

The DSI Host provides a scalable architecture using one or two data lanes.The number of lanes depends on the bandwidth requirements of the application. Each DSI lane has a maximum of 500 Mbit/s data rate, for a total 1Gbit/s rate in dual data lane mode.

Further information are detailed in AN4861application note it may help you.

-Nesrine-

Posted on October 17, 2017 at 16:29

Hi Nesrine,

You said 'using one or two data lanes'.

But my questions is whether you have any MCU with three data lanes?

Recommended app note does not mention about 3 lanes (only two)

Thanks

Posted on October 17, 2017 at 17:08

Hi

rostokus

,

Unfortunately,there is no STM32 device with 3 DSI data lanes, the STM32 embeded maximum 2 data lanes.

-Nesrine-