cancel
Showing results for 
Search instead for 
Did you mean: 

What is the Max DCMI Pixel Clock on the STM32H743 at 480 MHz? Is it 96MHz or fixed to 80 MHz?

MSale.1
Senior

As far as i understood the DCMI on AHB2 bus which has speed of (CPU/2 ) so at 480 MHz it will be 240MHz and the DCMI pixel clock must respect the minimum ratio of 2.5 so at this clock i will get 96 MHz or it for some other reason its fixed at 80 MHz only

0 REPLIES 0