2019-05-21 08:13 AM
Every text areas I place have cursor visible. From some of the areas I don't want to have cursors. How do I hide them?
2019-05-28 02:53 AM
Are you sure you cannot send me a modified project that exhibits this behavior?
2019-05-28 02:56 AM
No characters found in buffer.
I don't have the possibility to send a modified project right now. I'll try in a couple of weeks. :)
2019-05-28 02:59 AM
Could you try setting the width of the textareas to 0 and see if the "|" disappears?
2019-06-11 01:02 AM
Any update on this @Sandy.Dahl?
/Martin
2019-06-13 01:12 AM
I just noticed on your screenshot that the pipe on the bottom most input field seems to be "bold" - Can you verify that the typography used in that field is bold? Then we may be able to explain it.
2019-06-14 01:53 AM
I modified the title of this issue to: "Weird artifact showing in my TextAreaWithOneWildcard" to be more explicit.
2019-06-24 01:16 AM
Sorry, vacation causes long answer times. :)
The error has been found and solved, it was too easy to see. The character "|" was apparantely added in the assets/text/texts.xlsx-file...
Thanks for the help!
2019-06-25 05:39 AM
Okay, glad it was apparent :)
/Martin