2023-05-12 2:23 AM
In my project I have TouchGFX and USB (Virtual COM-Port) activated.
When generating code in STM32CubeMX, the USB Device files are placed under
"Middlewares/USB_Device_Library". Project compiles correct and is working.
After I generate code using TouchGFX Designer, these files are then missing and only touchgfx_core.lib is placed unter that item, which causes Linker Error for undefined symbols. I then have to manually add the files (usbd_core.c, usbd_ctlreq.c, usbd_ioreq.c and usbd_cdc.c) in a custom tree to keep them for further Generate Code cycles. But as soon as I regenerate Code with STM32CubeMX these files reappear in the Middlewares tree.
Please forward this to your "Generate Code" team for fixing the issue.
Thank you.
BR GS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.