2024-08-23 06:13 AM - last edited on 2024-08-23 08:11 AM by SofLit
Have seen in the community page that "TouchGFX can also be used on Linux, and even though the TouchGFX Designer cannot be run natively on Linux, the code generate by the TouchGFX Designer works on both Linux and Windows." but how , please help me in answering the below question that would help me:
1.Is it possible to edit the make file from the source code which generated by designer?
2.Is there a option to design screen for iMX boards?
3. What is the possible way to use TouchGFX for iMX boards like iMX8.
2024-08-23 07:47 AM
2024-08-23 08:00 AM - edited 2024-08-23 08:16 AM
Hello,
Almost same question in here https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/touchgfx-yocto-on-imx6-board-or-run-touchgfx-simulator-on-any/td-p/712122
TouchGFX designer and TouchGFX library are products of STMicroelectronics. TouchGFX library is exclusively compiled for STM32 products and it's internally protected for this kind of use case.
Thank you for your understanding.