2021-02-08 12:03 AM
In my previous post (Calling different functions when a button is pressed or released (Partially Solved): https://community.st.com/s/question/0D53W00000Wa1k2SAB/calling-different-functions-when-a-button-is-pressed-or-released-partially-solved ) I partially solved my problem by modifying the handlePressedUpdated() function.
But now I noticed a strange behavior: if I press/release the button all is OK, but if I press the button, swipe my finger out from the button area, and release, the button image become "unpressed" as soon I exit from the button area, but the "action on release" wasn't called.
I probably need to hook or modify the function that calls the changing of the button image by adding a function call, but I wasn't able to find that function (and I'm not sure it is the right way...).
Have a good day,
2021-02-08 4:39 AM
I mean this is normal touch reaction when you swipe you dont click simply, then release is filtered.
2021-02-08 5:20 AM
The problem is not when I swipe from an external zone to the button zone, but when I click the button, move away and release: the physical (not "software") LED controlled by the button stay glow UP.
Ok, but when I exit the button area, the button image switches from ON to OFF.
Well, I wish I "intercept" this signal to send the released button instruction also when you go out of the button zone to switching the LED off...
2021-02-09 9:23 AM
For the moment I adopt a "trivial" solution. I insert a "switch_off_all_LEDS()" directly in AbstractButtonContainer.hpp
virtual void handlePressedUpdated()
{
if (pressed==true)
{
button_pressed=true;
}
else{
button_pressed=false;
switch_off_all_LEDS();
}
}I'm looking for a better solution...